FS6500/FS4500 power efficency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6500/FS4500 power efficency

Jump to solution
4,111 Views
Jack_Zhao
Contributor II

Hi Sir,

     We are design a automotive project and has some questions for the efficency of FS6500 and 4500 as below, please kindly give your comment, thanks a lot:

1. As to FS6500: Are the vcore DC/DC, VCCA, VAUX and VCAN all generated by 6.5V;
   As to FS4500: Are the vcore LDO, VCCA, VAUX and VCAN all generated by 6.5V

2. Is the LDO efficency is calculated as below:
LDO input Voltage= 6.5V
5.0V output: 5/6.5=76.9%
3.3V output: 3.3/6.5=50.8%

3. What is the efficency in different load?
Vpre and Vcore

Light loads:
Out current
1mA=?
10mA=?
100mA=?

Normal loads:
300mA=?
500mA=?
700mA=?

It will be great appreciated if you can kindly recommend your light load but high efficency parts(for automotive) to us?

image (3).png

 

0 Kudos
Reply
1 Solution
4,016 Views
guoweisun
NXP TechSupport
NXP TechSupport

For VAUX used the external FETs which mean the FETs dissipation no calculate inside of SBC,so the efficiency will be higher.

View solution in original post

0 Kudos
Reply
7 Replies
4,103 Views
guoweisun
NXP TechSupport
NXP TechSupport

1. As to FS6500: Are the vcore DC/DC, VCCA, VAUX and VCAN all generated by 6.5V;
   As to FS4500: Are the vcore LDO, VCCA, VAUX and VCAN all generated by 6.5V

[gw]All input from VPRE.

2. Is the LDO efficency is calculated as below:
LDO input Voltage= 6.5V
5.0V output: 5/6.5=76.9%
3.3V output: 3.3/6.5=50.8%

[gw]No,you should use the Efficiency= VOUT*IOUT/(VIN*IIN).

3. What is the efficency in different load?
Vpre and Vcore

Light loads:
Out current
1mA=?
10mA=?
100mA=?

Normal loads:
300mA=?
500mA=?
700mA=?

It will be great appreciated if you can kindly recommend your light load but high efficency parts(for automotive) to us?

[gw] you can use the EVB to test the light load efficiency not too much data here:

guoweisun_0-1666156966153.pngguoweisun_1-1666156981732.png

 

0 Kudos
Reply
4,089 Views
Jack_Zhao
Contributor II

Hi GW,

     Per your comment: 1. VPER=6.5V; 2. LDO Efficiency= VOUT*IOUT/(VIN*IIN) and following the LDO feature IOUT=IIN, so LDO efficiency=VOUT/VIN(6.5V).

     For example, Vout=5V, LDO efficiency =5V/6.5V=76.9%

    Please correct me if i misunderstand your meaning.

    Thanks a lot.

0 Kudos
Reply
4,085 Views
guoweisun
NXP TechSupport
NXP TechSupport

No,the input current is not equal with output current for efficiency calculate.

 

 

0 Kudos
Reply
4,066 Views
Jack_Zhao
Contributor II
Hi GW
Do you have some efficiency data for VCCA, VAUX and VCAN?
It seems Vcca&Vaus are not pure LDO as what we know.
We would like to know the  efficiency for those ouput with light loads especially.
NXP web site has a tool:FS6500-FS4500 Power Dissipation Calculator  https://www.nxp.com.cn/downloads/en/calculators/FS6500-FS4500-power-dissipation-calculator.xlsx Could we refer to the excel file for efficency evaluation?
We calculated with this tool and found the efficency(Vcca and Vaux) is very high in light load such as 1mA-10mA.(the result is as below picture)
They should be Linear voltage regulator.
We are not sure if it is correct or not?
Could you help to double check?
Thanksimage (4).png
 
From Foxconn RD Qinguang and Jack
0 Kudos
Reply
4,028 Views
guoweisun
NXP TechSupport
NXP TechSupport

Yes, you can use  Power Dissipation Calculator  to estimate data.

 

0 Kudos
Reply
4,021 Views
Guang-Qin
Contributor II

Hi GW

We have doubts about the high efficiency of these two circuits (Vcca and Vaux). Is this really correct?

The efficiency does not change with the load. It is unreasonable. Can you help to confirm?

Another question is, They are  linear regulator, how can it achieve such high efficiency? ==> More than 99%?? It is unreasonable also.

 

FXN  Qin

0 Kudos
Reply
4,017 Views
guoweisun
NXP TechSupport
NXP TechSupport

For VAUX used the external FETs which mean the FETs dissipation no calculate inside of SBC,so the efficiency will be higher.

0 Kudos
Reply