FS65 Fault Error Counter incrementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS65 Fault Error Counter incrementation

ソリューションへジャンプ
4,306件の閲覧回数
razvan_simtion
Contributor II

Hello again,

I have a question regarding the incrementation of the fault error counter. Currently I am working with the FS65 in debug mode, after a couple of second in my code I change the answer to the LFSR in order to get a wdg error caused by data refresh, so far so good, the error counter increases until max as expected and after it restarts from 0 and so on. The problem is that the fault error counter does not increase, I have decided to change the WD_IMPACT_1:0 in  INIT_SF_IMPACT register from 00 (no effect on RSTB) to 01 (RSTB asserted if WD error counter reaches max val) in this formula the fault error counter increases when the error counter reaches its max val.

Any ideas regarding this issue? since according to the documentation the fault error counter should increase in any situation if the WD error counter = its max val not only with the workaround described above.

Also, I have noticed that I cannot read precisely when the error counter reaches its max value… for example if the max value is set to 6 the reading of WD_COUNTER register gives: 0x0F00, 0x0F40, 0x0F80 and then it jumps directly to 0: 0x0F00 . Can you confirm this is normal situation and it’s normal that I can’t read 0x0FC0 as max value, since in the manual it is stated that:” From 0 to 5 (6 generate an increase of the FLT_ERR_CNT and this counter is reset to 0)”

Thank you in advance!

Kind Regards,

Razvan Simtion

ラベル(1)
タグ(2)
1 解決策
4,139件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Razvan,

As shown in chapter 6.5.3 of the datasheet, the fault error counter is increased in two situations:

pastedImage_1.png

When you set WD_IMPACT_1:0 = 0b00, there is no RSTB /FS0B assertion when the watchdog error counter reaches the max value, so the fault error counter will not increase.

As for your second question, yes, the watchdog error counter does not show 6 as it goes to 0 when the max value is reached.

pastedImage_104.png

pastedImage_105.png

Best regards,

Tomas

元の投稿で解決策を見る

2 返答(返信)
4,140件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Razvan,

As shown in chapter 6.5.3 of the datasheet, the fault error counter is increased in two situations:

pastedImage_1.png

When you set WD_IMPACT_1:0 = 0b00, there is no RSTB /FS0B assertion when the watchdog error counter reaches the max value, so the fault error counter will not increase.

As for your second question, yes, the watchdog error counter does not show 6 as it goes to 0 when the max value is reached.

pastedImage_104.png

pastedImage_105.png

Best regards,

Tomas

4,139件の閲覧回数
razvan_simtion
Contributor II

Hello Tomas,

Thank you for the clarification. 

I have read the documentation and what made me doubt was the section:

fault_err.PNG

0 件の賞賛
返信