FS4503 Grounding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,820件の閲覧回数
wade_liu
Contributor I

Hello!

Please help us clarify the following questions

1. Witch pin the return path of GATE_LS?(AGND or DGND)

2. GND of S32K144 is no distinction between digital and analog (No DGND,AGND, Only Vss), How do you recommend grounding while we use FS4503 & S32K144?

Thank you!!

ラベル(1)
0 件の賞賛
返信
1 解決策
3,680件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

[A1] Return path of GATE_LS is AGND. But at the end you can connect all the ground together as in the schematic in the following link: https://www.nxp.com/downloads/en/schematics/FRDMFS4503CAEVM-A-SCH.pdf

 

[A2] S32K144 have VSS (Ground) and VSSA (Analog Ground), but both must be shorted to a general GND at package level.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,681件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

[A1] Return path of GATE_LS is AGND. But at the end you can connect all the ground together as in the schematic in the following link: https://www.nxp.com/downloads/en/schematics/FRDMFS4503CAEVM-A-SCH.pdf

 

[A2] S32K144 have VSS (Ground) and VSSA (Analog Ground), but both must be shorted to a general GND at package level.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,680件の閲覧回数
wade_liu
Contributor I

Thank you for your information!

So, that's mean the return path of 12V battery (VSUP1/2) is also AGND?

I will connect AGND & DGND together, but I'm thinking about where to place common point on the PCB layout.

0 件の賞賛
返信
3,680件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Wade,

 

Correct, the return path of 12V battery (VSUP1/2) is also AGND.

Connecting the AGND & DGND together can be done by placing an inductor (around 1uH or less) between them.

 

Regards,

Jose