FS26 VCORE setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 VCORE setting

4,379 Views
e2s
Contributor I

Dear team,

 

how can the VCORE voltage be set on the FS26? We want to realize VCORE=1.2V.

Are there any feedback resistors necessary on the CORE_FB input?

What is the internal reference of the CORE_FB pin?

Or is this device dependent by ordering code?

Best regards,

Jochen

0 Kudos
Reply
4 Replies

4,344 Views
e2s
Contributor I

Hello team,

 

I have opened the AN12995, Rev1, 9 March 2023. Chapter 3.5 does not exist.

 

Chapter 4.5 shows this drawing. Now again the question - how can the Core voltage be set?

0 Kudos
Reply

4,337 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Sure, let me explain. 

VCORE is a synchronous buck converter with integrated FETs. VCORE is dedicated for microcontroller core supply. Output DC current up to 0.8 A or 1.65 A (depending on part number).

 

ErikaC_1-1719334818965.png

Output voltage range setting from 0.8 V to 3.35 V (OTP configuration, 10 mV step) which will be modified from the OTP configuration, please see OTP_CORE_VOLT1 register bit description.

ErikaC_2-1719334993538.png

 

So, if you want Core voltage to 1.2V use 28h.

0 Kudos
Reply

4,327 Views
e2s
Contributor I

Hello team,

 

OK, understood. For development purposes this is a way.

But how is the FS26 with VCORE=1.2V and OTP_CORE_VOLT1=0x28 in series production to be identified? With a special part number?

0 Kudos
Reply

4,356 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Please find the information in the Application note AN12995, chapter 3.5 Vcore Regulator.

Note: The document is under secure files.

0 Kudos
Reply