FS26 TRK2_UV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 TRK2_UV

8,397件の閲覧回数
dingyazhou
Contributor I

Hello, my FS26 will report TRK2_UV failure at the INIT_FS stage of the chip, so it cannot exit the INIT_FS stage, and the functional safety state machine is stuck. May I ask what is the cause

0 件の賞賛
返信
15 返答(返信)

5,764件の閲覧回数
Vendrick
Contributor I

hi how can i use the VCORE to supply the VDD_LV of the MCP5746C

 

0 件の賞賛
返信

8,383件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

So for your FS26 setting TRK2_V_OTP [1:0] = 11 as 5.5V and actually it only has 5V,so it trigger UV threshold,right?

0 件の賞賛
返信

6,793件の閲覧回数
459021854
Contributor III
  • Hi, have you got the SCH-47651 schematics, if you have, can you share with me. Thanks
0 件の賞賛
返信

6,798件の閲覧回数
459021854
Contributor III

Hi, have you got the SCH-47651 schematics, if you have, can you share with me. Thanks

0 件の賞賛
返信

8,377件の閲覧回数
dingyazhou
Contributor I

It may be so, but the agent did not provide the documents for OTP configuration when buying the board. The model of FS26 is FS26AMDA0A1, and the model of development board is SCH-47651 REV A1

0 件の賞賛
返信

8,373件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Understand, so you can  test the voltage of VTRK2 to confirm this voltage level and tell me the result.

0 件の賞賛
返信

8,386件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

what's the value of TRK2 in your board now? do you test it?

0 件の賞賛
返信

8,384件の閲覧回数
dingyazhou
Contributor I

As explained below, TRK2 and TRK1 are both 5V, now TRK2 will have an undervoltage flag to read the FS_OVUV_REG_STATUS register through SPI

0 件の賞賛
返信

8,379件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Could you please share with your schematic?

0 件の賞賛
返信

8,371件の閲覧回数
dingyazhou
Contributor I

dingyazhou_0-1633759518620.jpeg

 

0 件の賞賛
返信

8,349件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

During the initialization phase, you can try to set VMON_TRK2_UV_FS_REACTION [1:0 ] as 00 to disable safety output and RSTB based on register of FS_I_OVUV_SAFE_REACTION2.

Use this method to eliminate the TRK2 UV affect.

0 件の賞賛
返信

8,361件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Can you share the circuit of SCH-47651?

0 件の賞賛
返信

8,353件の閲覧回数
dingyazhou
Contributor I

Can you add a wechat for easy communication: 18196548686

dingyazhou_0-1633760502504.jpeg

 

0 件の賞賛
返信

8,394件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please measure the actual value of TRK2 and check whether the short circuit happened or not?

0 件の賞賛
返信

8,391件の閲覧回数
dingyazhou
Contributor I

The voltage of TRK2 and TRK1 is 5V, and now it is TRK2 undervoltage fault stuck functional safety state machine. The chip manual has such a sentence:  If the regulator is used as a global pin, outside of the module, it is recommended to not include it in power up sequence and turn on the regulator by SPI, to avoid a stuck in reset condition in case of short circuit.

0 件の賞賛
返信