FS26 ABIST

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 ABIST

Jump to solution
735 Views
90insu
Contributor II

Is ABIST for FS26 automatically provided from the IC itself? or Do we need to configure it prior to receiving IC like OTP?

0 Kudos
Reply
1 Solution
729 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Insoo,

ABIST is fully integrated inside the FS26 and is automatically available in the device. ABIST1 runs automatically at startup as part of the device’s internal safety checks. ABIST2 is available as an on‑demand test and can be triggered later during normal operation via SPI.
 
OTP is only used to configure the behavior and reactions related to ABIST, for example which domains or monitors participate and how the device reacts if an ABIST failure occurs (FS outputs, reset behavior, fault handling).
 
BRs, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
730 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Insoo,

ABIST is fully integrated inside the FS26 and is automatically available in the device. ABIST1 runs automatically at startup as part of the device’s internal safety checks. ABIST2 is available as an on‑demand test and can be triggered later during normal operation via SPI.
 
OTP is only used to configure the behavior and reactions related to ABIST, for example which domains or monitors participate and how the device reacts if an ABIST failure occurs (FS outputs, reset behavior, fault handling).
 
BRs, Tomas
0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2358607%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EFS26%20ABIST%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2358607%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EIs%20ABIST%20for%20FS26%20automatically%20provided%20from%20the%20IC%20itself%3F%20or%20Do%20we%20need%20to%20configure%20it%20prior%20to%20receiving%20IC%20like%20OTP%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2358628%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20FS26%20ABIST%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2358628%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%20Insoo%2C%3C%2FP%3E%0A%3CDIV%3EABIST%20is%20fully%20integrated%20inside%20the%20FS26%20and%20is%20automatically%20available%20in%20the%20device.%26nbsp%3BABIST1%20runs%20automatically%20at%20startup%20as%20part%20of%20the%20device%E2%80%99s%20internal%20safety%20checks.%20ABIST2%20is%20available%20as%20an%20on%E2%80%91demand%20test%20and%20can%20be%20triggered%20later%20during%20normal%20operation%20via%20SPI.%3C%2FDIV%3E%0A%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%0A%3CDIV%3EOTP%20is%20only%20used%20to%20configure%20the%20behavior%20and%20reactions%20related%20to%20ABIST%2C%20for%20example%20which%20domains%20or%20monitors%20participate%20and%20how%20the%20device%20reacts%20if%20an%20ABIST%20failure%20occurs%20(FS%20outputs%2C%20reset%20behavior%2C%20fault%20handling).%3C%2FDIV%3E%0A%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%0A%3CDIV%3EBRs%2C%20Tomas%3C%2FDIV%3E%3C%2FLINGO-BODY%3E