FS23 V1 output abnormal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS23 V1 output abnormal

1,352 Views
seerlu
Contributor I

V1 output is abnormal as below waveform:

C1 was VSUP,C2 was VBOS,C3 was V2;C4 was V1(power to MCU)C1 was VSUP,C2 was VBOS,C3 was V2;C4 was V1(power to MCU)微信图片_20260813093846_286_23.jpgV1 without npnV1 without npn微信图片_2026-08-13_095130_111.png

How can I thoroughly solve the problems I am currently facing?

if you want to get more information,please let me know.

0 Kudos
Reply
13 Replies

1,343 Views
seerlu
Contributor I

VBOS>3.06V TO V1 UPing used 13.2msVBOS>3.06V TO V1 UPing used 13.2ms

0 Kudos
Reply

1,345 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can try to disconnect  MCU with V1 and test it again for example add some loading 50mA. 

0 Kudos
Reply

1,315 Views
seerlu
Contributor I

This is testing.

by the way, we check the manual and found 19.4.6 V1UVLP monitoring chapter shows "V1 is also monitored for V1UVLP when the device powers up after a wake up from LPON, and during a cold start after TSOFT_START_V1. If, at the end of the softstart, V1 is still under V1UVLP threshold, then the device goes into Fail-Safe state."

does it mean V1 should beyond V1UVLP threshold after TSOFT_START_V1(type,300us)?

 

in addition ,this V1 abnormal issue happened in low temperature (-30℃ ) and low Vsup power(8v)。in this condition, we increased VSUP to 12V,V1 output OK。

0 Kudos
Reply

1,312 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1786601048119.png

guoweisun_1-1786601077374.png

A lots of confuse for your test result ,you can see when Vbat< Vsup_uv,the V1 should be stay 0,why your V1 follow up VBAT from 0? I suppose your test waveform yellow is VBAT,Green is V1,am I right?

0 Kudos
Reply

1,306 Views
seerlu
Contributor I
Channel 1 was VSUP,C2 was VBOS,C3 was V2;C4 was V1(power to MCU)
0 Kudos
Reply

1,309 Views
seerlu
Contributor I
which one indicate V1 follow up VBAT from 0?
current test results show VBOS>3.06V TO V1 UPing used 13.2ms, please check
0 Kudos
Reply

1,288 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1786608712650.png

在8V Vin的情况下能否把这个上面圈出来的波形的时间轴放小些,我想看V1启动了多久?

另外12V VIN的情况下也测试下相同的波形可以嘛?

我这里没有高低温试验箱无法做太多的测试只能看你们的结果了。

0 Kudos
Reply

1,272 Views
seerlu
Contributor I

我们新测了个波形,在输入12V时也发现V1有时第一次启动是失败的。

af12f0f0-afa6-40e3-881d-890516697b5a.png

这是第一次启动失败的波形V1第一次启动未成功图V1第一次启动未成功图

这是第二次启动成功的波形V1第二次启动成功图V1第二次启动成功图

 

这个是不是和那个V1 在软启动之后的欠压检测有关联,但是软启动的时间是典型值300,最大值500us。现在为啥感觉是超过500us就启动不起来,低于500us好像就行。

能否帮忙描述下软启动的内容,看手册没有太多描述

0 Kudos
Reply

1,224 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个问题大概率是V1 发生了OC在软启动的过程中导致启动失败然后又恢复的这个过程。

解决方案可以外加管子阔流在V1端口然后FS23 OTP的时候把这个功能打开,也可以选择我们的HVBUCK的版本。

要么就是适当的去掉一些输出电容让softstart更顺畅,我建议选择上面两个方案更稳妥

 

 

0 Kudos
Reply

1,221 Views
seerlu
Contributor I

能否帮忙在解释下softstart过程?

包括这一段“19.4.6 V1UVLP monitoring chapter shows "V1 is also monitored for V1UVLP when the device powers up after a wake up from LPON, and during a cold start after TSOFT_START_V1. If, at the end of the softstart, V1 is still under V1UVLP threshold, then the device goes into Fail-Safe state."”到底是要求什么样的V1启动波形?

 

谢谢

0 Kudos
Reply

1,218 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1786680381549.png

guoweisun_1-1786680552393.png

 

这个图可以解释框出来的上面的是softstart的条件,假如都满足了V1开始上电了进入M5的时序,他的时间是150-500us,假如超过了这个时间还没有启动成功就会进入FS状态然后100ms以后重启这样一个大概的过程

 

0 Kudos
Reply

1,231 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:原理图PIN37不用的话接地。

2:V1的负载电流不大的最大才100mA确认下您那里的负载

3:V1_IN的decouple 电容是1uF.

guoweisun_0-1786671133675.png

4: 就像上面这个情况第一次启动不成功第二次起来了能否读取寄存器 M_GEN_FLAG register 看看发生了什么?

先改上面这些看看结果。

 

 

0 Kudos
Reply

1,306 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can see below circled part.

guoweisun_0-1786601658488.png

 

0 Kudos
Reply