Continued Sleep - Wakeup cycle with MC33771C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Continued Sleep - Wakeup cycle with MC33771C

1,239件の閲覧回数
EmbeddedExpert
Contributor II

Is it possible to keep the MC33771C in a continuous sleep / wakeup cycle unless an error occurred?

I can see that it sleeps for the selected timed (e.g. 8sec) and then it wakes up for measurement cycle.

Even if all wakeup masks are set (to disable)  there is a wakeup pulse (TPL) to the MC33664.

Is there a way to keep the MC33771C in a cyclic loop without MCU interaction?

 

タグ(4)
0 件の賞賛
返信
1 返信

1,183件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Seems that it still need MCU to  interaction.

0 件の賞賛
返信