flexio SPI for S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexio SPI for S32K144

2,150 Views
mogilipuri_harish
Contributor II

hello team,

 

we are using S32K144 64 pin package uC in our design. so we are using FlexIO SPI for as a slave configuration. 

as mentioned below pins we are using SPI slave mode 

PINSPin Names
3FlexIO SPI slave in Pin:FlexIO_D5 
4FlexIO SPI slave out Pin:FlexIO_D4
5FlexIO SPI slave CS Pin:FlexIO_D7
6FlexIO SPI slave SCK Pin:FlexIO_D6

 

from the master side SPI fixed to Mode3 (i.e CPOL = 1 and CPHA = 1). so for uC FlexIO will support for Mode 3.

can please share the FlexIO timing diagram?

is there any limitation in FlexIO compared stadard LPSPI? 

 

0 Kudos
Reply
2 Replies

2,107 Views
mogilipuri_harish
Contributor II

The driver does not support back-to-back transmission mode for CPHA = 1. 

this means it will not works continuously in this mode

0 Kudos
Reply

2,135 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @mogilipuri_harish 

There is not like timing diagram but in the references manual section 54.5.4(SPI Slave) the necessary configurations, also, there is an application note that shows how to emulate communications and timing peripherals.

AN12174: Using FlexIO to emulate communications and timing peripherals – Application Note

AN12174SW, Application note software for AN12174

 

B.R.

VaneB

0 Kudos
Reply