Built In Self Tests in FS85

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Built In Self Tests in FS85

2,424 Views
haby_a
Contributor II

What will happen when ABIST or LBIST tests fail in FS85. I understand that FS0B pin will be stuck low. How does FS85 behave after this; will watchdog windowing happens and refresh will be accepted by FS85 without shifting to normal mode? or will RSTB pin be asserted?

Also how ABIST2 test is launched via SPI ? Is it done by configuring FS_I_OVUV_SAFE_REACTION1 register during INIT_FS?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,270 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Haby,

Yes, if ABIST1 (ABIST1_OK = 0) or LBIST (LBIST_OK = 0) fails, RSTB and PGOOD are released, but FS0B remains stuck low keeping the application in safe state. The Fail-safe state machine transitions to the INIT_FS state as usual.

 

As for the ABIST2, during INIT_FS, the MCU configures the ABIST2 coverage with the FS_I_OVUV_SAFE_REACTION1 register, assigning the voltage monitoring to be verified during ABIST2:

 

  • VCOREMON_ABIST2 = 1 to verify VCOREMON comparators during ABIST2
  • VDDIOMON_ABIST2 = 1 to verify VDDIOMON comparators during ABIST2
  • VMONx_ABIST2 = 1 to verify VMONx comparators during ABIST2

pastedImage_2.png

pastedImage_3.png

pastedImage_5.png

 

As soon as INIT_FS is closed and the latest voltage regulator assigned to ABIST2 is started, ABIST2 is executed.

Best regards,

Tomas

0 Kudos
Reply