BMS IC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BMS IC

1,623件の閲覧回数
Diwakar415
Contributor I

Hello NXP Experts,

I'm designing a BMS for 3S2P cells in series and parallel, where entire pack is 11.1V, 5000mAH.

I should achieve over voltage protection(12.6v), under voltage protection(9v), over current protection and short circuit protection.

And My charge current should be less than 5A and Discharge current should be less than 8A.

can you please suggest me IC for this requirement and its evaluation Board.

Regards,

Diwakar.B

0 件の賞賛
返信
1 返信

1,609件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

In this case, I would like to recommend the series below:

MC33771B - 14-Channel Li-Ion Battery Cell Controller IC

The MC33771 Li-ion battery cell controller IC designed for automotive and industrial applications such as 48 V Li-ion batteries, HEV, EV, ESS, UPS systems.

From the webpage provided, please go to the Hardware section in order to review all the evaluation boards available.

diazmarin09_0-1674253739671.pngdiazmarin09_0-1674253739671.png

 

I hope this information helps.

Regards,

David

0 件の賞賛
返信