Application note for implementing TEA1721AT in design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Application note for implementing TEA1721AT in design

672件の閲覧回数
tkoha
Contributor I

I need to build a fly-back converter with 2 isolated outputs and with an input range of 19 - 150Vdc. It also needs to have a VERY no-load consumption.

I was therefore looking at the TEA1721 family.

Is there a tool or application note that can help me with this design?

0 件の賞賛
返信
1 返信

655件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

That's not easy for design this  by use one stage power solution because the input range is more special.

You can use one stage BOOST to improve input voltage into 150V or above,then second stage use the normal fly-back or QR FLYBACK controller to get the isolation solution.

You can calculate by following attached calculate sheet. for QR FLY-BACK  topology.

Hope this could help!

 

0 件の賞賛
返信