Application note for implementing TEA1721AT in design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Application note for implementing TEA1721AT in design

692 次查看
tkoha
Contributor I

I need to build a fly-back converter with 2 isolated outputs and with an input range of 19 - 150Vdc. It also needs to have a VERY no-load consumption.

I was therefore looking at the TEA1721 family.

Is there a tool or application note that can help me with this design?

0 项奖励
回复
1 回复

675 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

That's not easy for design this  by use one stage power solution because the input range is more special.

You can use one stage BOOST to improve input voltage into 150V or above,then second stage use the normal fly-back or QR FLYBACK controller to get the isolation solution.

You can calculate by following attached calculate sheet. for QR FLY-BACK  topology.

Hope this could help!

 

0 项奖励
回复