uboot access mac register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot access mac register

3,102 Views
longqiluo
Contributor II

hello,We designed board  based on the p1023rds . And the etherent part of it is completely refered to the ethernet part of P1023RDS. But I am confusing about MAC register access.could someone tell me how to read/write dtsec1 mac register by uboot cammand?the CCSR baseaddr=0xff600000

Labels (1)
0 Kudos
Reply
4 Replies

2,761 Views
Pavel
NXP Employee
NXP Employee

Offset 0x4e_0000 correct for the P5020/P3041/P2041. The P1023 offset is 0x1E_0000.

The P1023RDS MAC address is available using the following command:

=> md ff7e0100

ff7e0100: 00000000 00007215 40605060 00a1f037    ......r.@`P`...7

ff7e0110: 00000800 00000000 00000000 00000000    ................

ff7e0120: 00000000 00000000 00000000 00000000    ................

ff7e0130: 00000000 00000000 01000000 00000008    ................

ff7e0140: 345b009f 04000000 00000000 00000000    4[..............

ff7e0150: 00000000 00000000 00000000 00000000    ................

ff7e0160: 00000000 00000000 00000000 00000000    ................

ff7e0170: 00000000 00000000 00000000 00000000    ................

ff7e0180: 00000000 00000000 00000000 00000000    ................

ff7e0190: 00000000 00000000 00000000 00000000    ................

ff7e01a0: 00000000 00000000 00000000 00000000    ................

ff7e01b0: 00000000 00000000 00000000 00000000    ................

ff7e01c0: 00000000 00000000 00000000 00000000    ................

ff7e01d0: 00000000 00000000 00000000 00000000    ................

ff7e01e0: 00000000 00000000 00000000 00000000    ................

ff7e01f0: 00000000 00000000 00000000 00000000:

 

MAC address for our board is the following:

ethaddr=00:04:9F:00:5B:34

 

> printenv

baudrate=115200

bootargs=root=/dev/ram console=ttyS0,115200

bootcmd=nand read 1000000 200000 400000;nand read c00000 100000 4000;nand read 2000000 600000 1A00000;bootm 1000000 2000000 c00000

bootdelay=3

bootfile=uImage

console=,115200

eth1addr=00:04:9F:00:5B:35

eth2addr=00:04:9F:00:5B:36

ethact=FM1@DTSEC1

ethaddr=00:04:9F:00:5B:34

fdtaddr=c00000

fdtfile=p1023rdb.dtb

fman_ucode=0x7f933638

gatewayip=192.168.3.64

hostname=P1023RDB

ipaddr=192.168.2.104

loadaddr=1000000

netdev=eth0

netmask=255.255.254.0

nfsargs=setenv bootargs root=/dev/nfs rw nfsroot=192.168.2.111:/tftpboot/yocto ip=192.168.2.104:192.168.2.111:192.168.2.64:255.255.254.0:P1023RDB:eth0:off

nfsboot=run nfsargs;tftp 1000000 uImage;tftp c00000 p1023rdb.dtb;bootm 1000000 - c00000

rootpath=/tftpboot/yocto

serverip=192.168.3.64

stderr=serial

stdin=serial

stdout=serial


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,761 Views
longqiluo
Contributor II

OK ,thank you! is very useful!

a

body {

font-family: Helvetica, Arial, sans-serif;

-webkit-text-size-adjust: 100%;

}

/* Webkit */

h1, h2, h3, h4, h5, h6, p, hr {

-webkit-margin-before: 0;

-webkit-margin-after: 0;

-webkit-margin-start: 0;

-webkit-margin-end: 0;

}

.button td {

background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0

51%, #387AC8 100%) !important;

background-image: -webkit-gradient(linear, left top, left bottom, color-stop(

0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#

387AC8)) !important;

-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !

important;

-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

}

Pavel 写:

NXP Community

Re: uboot access mac register

reply from Pavel Chubakov in QorIQ Processing Platforms - View the full

discussion

Offset 0x4e_0000 correct for the P5020/P3041/P2041. The P1023 offset is

0x1E_0000.The P1023RDS MAC address is available using the following command:=&

gt; md ff7e0100ff7e0100: 00000000 00007215 40605060 00a1f037 ......r.@`P`...

7ff7e0110: 00000800 00000000 00000000 00000000 ................ff7e0120:

00000000 00000000 00000000 00000000 ................ff7e0130: 00000000

00000000 01000000 00000008 ................ff7e0140: 345b009f 04000000

00000000 00000000 4[..............ff7e0150: 00000000 00000000 00000000

00000000 ................ff7e0160: 00000000 00000000 00000000 00000000 ...

.............ff7e0170: 00000000 00000000 00000000 00000000 ................

ff7e0180: 00000000 00000000 00000000 00000000 ................ff7e0190:

00000000 00000000 00000000 00000000 ................ff7e01a0: 00000000

00000000 00000000 00000000 ................ff7e01b0: 00000000 00000000

00000000 00000000 ................ff7e01c0: 00000000 00000000 00000000

00000000 ................ff7e01d0: 00000000 00000000 00000000 00000000 ...

.............ff7e01e0: 00000000 00000000 00000000 00000000 ................

ff7e01f0: 00000000 00000000 00000000 00000000: MAC address for our board is the

following: ethaddr=00:04:9F:00:5B:34 > printenvbaudrate=115200bootargs=root=/

dev/ram console=ttyS0,115200bootcmd=nand read 1000000 200000 400000;nand read

c00000 100000 4000;nand read 2000000 600000 1A00000;bootm 1000000 2000000

c00000bootdelay=3bootfile=uImageconsole=,115200eth1addr=00:04:9F:00:5B:

35eth2addr=00:04:9F:00:5B:36ethact=FM1@DTSEC1ethaddr=00:04:9F:00:5B:34fdtaddr=

c00000fdtfile=p1023rdb.dtbfman_ucode=0x7f933638gatewayip=192.168.3.64hostname=

P1023RDBipaddr=192.168.2.104loadaddr=1000000netdev=eth0netmask=255.255.254.

0nfsargs=setenv bootargs root=/dev/nfs rw nfsroot=192.168.2.111:/tftpboot/yocto

ip=192.168.2.104:192.168.2.111:192.168.2.64:255.255.254.0:P1023RDB:eth0:

offnfsboot=run nfsargs;tftp 1000000 uImage;tftp c00000 p1023rdb.dtb;bootm

1000000 - c00000rootpath=/tftpboot/yoctoserverip=192.168.3.64stderr=serialstdin=

serialstdout=serial

Have a great day,

Pavel Chubakov

0 Kudos
Reply

2,761 Views
Pavel
NXP Employee
NXP Employee

Use md - memory display command of the u-boot. See md command description of the u-boot on the following page:http://www.denx.de/wiki/view/DULG/UBootCmdGroupMemory#Section_5.9.2.5. 

The P1023 dTSEC1 Block base addresses is 0x4E_0000. See the Section 18.3.3 of the P1023 Reference Manual. Look at the dTSEC Ethernet Module Memory Map in the Table 3-8 of the QorIQ Data Path Acceleration Architecture (DPAA) Reference (REV 2):

https://www.nxp.com/webapp/Download?colCode=DPAARM&location=null&fsrch=1&sr=4&pageNum=1&Parent_nodeI...

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,761 Views
longqiluo
Contributor II

hello, I don't know what's meaning of the DTSEC1 block base addrss (4e_0000),

but I access DTSEC memory-map register by reading and writing an address

consisting of the CCSR(ff600000) plus the fman block(100000), plus the offset

of specific register to be accessed , as below,. So what is the DTSCE1 block

base address 4e0000 used for ? The dtsec1 still not work ,pleaese analyze for

me=> base ff7e0000Base Address: 0xff7e0000=> md 0 3fff7e0000: 08240101

002c0000 02000700 00000000 .$...,..........ff7e0010: 00000000 00000058

00000000 00000008 .......X........ff7e0020: 00000000 00000000 00000000

00000000 ................ff7e0030: 00000000 00000000 00000000 00000000 ...

.............ff7e0040: 00000020 00000000 00000000 00000000 ... ............

ff7e0050: 00000021 00000000 00000000 00000000 ...!............ff7e0060:

00000000 00000000 00000000 00000000 ................ff7e0070: 00000000

00000000 00000000 00000000 ................ff7e0080: 00000000 00000000

00000000 00000000 ................ff7e0090: 00000000 00000000 00000000

00000000 ................ff7e00a0: 00000000 00000000 00000000 00000000 ...

.............ff7e00b0: 00000000 00000000 00000000 00000000 ................

ff7e00c0: 00000000 00000000 00000000 00000000 ................ff7e00d0:

00000000 00000000 00000000 00000000 ................ff7e00e0: 00000000

00000000 00000000 00000000 ................ff7e00f0: 00000000 00000000

00000000 ............=> md 0 2ff7e0000: 08240101 002c0000 .$...,..=>

md 100 44ff7e0100: 00000000 00007115 40605060 00a1f037 ......q.@`P`...

7ff7e0110: 00000800 00000000 00000000 00000000 ................ff7e0120:

00000000 00000000 00000000 00000000 ................ff7e0130: 00000000

00000000 01000000 00000008 ................ff7e0140: 00000000 00000000

00000000 00000000 ................ff7e0150: 00000000 00000000 00000000

00000000 ................ff7e0160: 00000000 00000000 00000000 00000000 ...

.............ff7e0170: 00000000 00000000 00000000 00000000 ................

ff7e0180: 00000000 00000000 00000000 00000000 ................ff7e0190:

00000000 00000000 00000000 00000000 ................ff7e01a0: 00000000

00000000 00000000 00000000 ................ff7e01b0: 00000000 00000000

00000000 00000000 ................ff7e01c0: 00000000 00000000 00000000

00000000 ................ff7e01d0: 00000000 00000000 00000000 00000000 ...

.............ff7e01e0: 00000000 00000000 00000000 00000000 ................

ff7e01f0: 00000000 00000000 00000000 00000000 ................ff7e0200:

00000000 00000000 00000000 00000000 ................=>

a

body {

font-family: Helvetica, Arial, sans-serif;

-webkit-text-size-adjust: 100%;

}

/* Webkit */

h1, h2, h3, h4, h5, h6, p, hr {

-webkit-margin-before: 0;

-webkit-margin-after: 0;

-webkit-margin-start: 0;

-webkit-margin-end: 0;

}

.button td {

background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0

51%, #387AC8 100%) !important;

background-image: -webkit-gradient(linear, left top, left bottom, color-stop(

0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#

387AC8)) !important;

-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !

important;

-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

}

Pavel 写:

NXP Community

Re: uboot access mac register

reply from Pavel Chubakov in QorIQ Processing Platforms - View the full

discussion

Use md - memory display command of the u-boot. See md command description of

the u-boot on the following page:http://www.denx.de/wiki/view/DULG/

UBootCmdGroupMemory#Section_5.9.2.5. The P1023 dTSEC1 Block base addresses is

0x4E_0000. See the Section 18.3.3 of the P1023 Reference Manual. Look at the

dTSEC Ethernet Module Memory Map in the Table 3-8 of the QorIQ Data Path

Acceleration Architecture (DPAA) Reference (REV 2):https://www.nxp.com/webapp/

Download?colCode=DPAARM&location=null&fsrch=1&sr=4&pageNum=1&

amp;Parent_nodeId=&Parent_pageType= Have a great day,

Pavel Chubakov

0 Kudos
Reply