p4080ds usdpaa can't be tested

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p4080ds usdpaa can't be tested

3,610件の閲覧回数
gaolixing
Contributor I

hello,my p4080ds linux sdk source code is download from https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk project

now i want to use usdpaa function with p4080,but i can't find p4080ds-usdpaa.dts in my source code,and i can't find example source code for usdpaa such as usdpaa-apps,how can i get the source code for reflector application,sra application and so on.

is it the linux sdk source code download from https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk don't support usdpaa? usdpaa is very import for me.

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

3,525件の閲覧回数
gaolixing
Contributor I

thanks ‌,i have install "QorIQ Linux SDK v2.0 SOURCE.iso" and  "QorIQ SDK V2.0 PPCE500MC Yocto CACHE.iso" in the same path,i also resolved the two build problems:

[yocto] [pyro][bitbake][PATCH] bitbake: Replace deprecated git branch parameter "--set-upstream" 

[pseudo-native] No real function for mknod 

but when i build the linux system,the follow is errors:

branch 'origin/sdk-v2.0.x' does not exist

Task 1331 (/home/linux-develop/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-dpaa/usdpaa/usdpaa_git.bb, do_unpack) failed with exit code '1'

i guess the error is about " git -c core.fsyncobjectfiles=0 branch --set-upstream-to sdk-v2.0.x origin/sdk-v2.0.x"

how can i resolve the problem?

0 件の賞賛
返信

3,525件の閲覧回数
gaolixing
Contributor I

i have  login www.nxp.com,

Screenshot from 2020-06-03 16-36-47.png

i don't find QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500MC-CACHE-20160527-yocto.iso

0 件の賞賛
返信

3,525件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download

"QorIQ Linux SDK v2.0 SOURCE.iso" and 

"QorIQ SDK V2.0 PPCE500MC Yocto CACHE.iso"

0 件の賞賛
返信

3,525件の閲覧回数
gaolixing
Contributor I

thank you,but where can i download  ISO QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500MC-CACHE-20160527-yocto.iso? i don't find them at Linux® SDK for QorIQ® Processors | NXP

0 件の賞賛
返信

3,525件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please login www.nxp.com, then click "Download" from the above link.

0 件の賞賛
返信

3,525件の閲覧回数
gaolixing
Contributor I

my image boot log display "QorIQ SDK (FSL Reference Distro) 2.7+snapshot p4080ds ttyS0",is that meaning the version of yocto is 2.7?

0 件の賞賛
返信

3,525件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello lixing gao,

Please download source ISO QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500MC-CACHE-20160527-yocto.iso, then install both ISOs in the same path, you could build images without networking connection.

Thank,

Yiping

0 件の賞賛
返信

3,525件の閲覧回数
gaolixing
Contributor I

thanks for your reply,but QorIQ Linux SDK 2.0 release, which could be downloaded from Linux® SDK for QorIQ® Processors | NXP can't be compiled because www.freescale.com is shut down,which yocto verison support both

p4080ds and USDPAA

0 件の賞賛
返信

3,525件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello lixing gao,

Yocto 3.0 release doesn't support USDPAA, you could use QorIQ Linux SDK 2.0 release, which could be downloaded from Linux® SDK for QorIQ® Processors | NXP .

Thanks,

Yiping

0 件の賞賛
返信