external Watchdog timer program to reset the P2020

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

external Watchdog timer program to reset the P2020

2,385件の閲覧回数
nareshpuli
Contributor III

hi,

i am trying to write a program for external watchdog timer , to reset the P2020 processor, help me.

how we write the program ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,089件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple watchdog program example for the MPC8548. See the main.c file. The P2020 watchdog is the same as the MPC8548. Similar code can be used on the P2020 board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,089件の閲覧回数
nareshpuli
Contributor III

Hi Pavel Chubakov,

thanks for your reply, where is attached file, i can't find.

Regards

Naresh

Have a nice day...

0 件の賞賛
返信

2,089件の閲覧回数
nareshpuli
Contributor III

i got it...

0 件の賞賛
返信