external Watchdog timer program to reset the P2020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

external Watchdog timer program to reset the P2020

2,387 Views
nareshpuli
Contributor III

hi,

i am trying to write a program for external watchdog timer , to reset the P2020 processor, help me.

how we write the program ?

Labels (1)
0 Kudos
Reply
3 Replies

2,091 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple watchdog program example for the MPC8548. See the main.c file. The P2020 watchdog is the same as the MPC8548. Similar code can be used on the P2020 board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,091 Views
nareshpuli
Contributor III

Hi Pavel Chubakov,

thanks for your reply, where is attached file, i can't find.

Regards

Naresh

Have a nice day...

0 Kudos
Reply

2,091 Views
nareshpuli
Contributor III

i got it...

0 Kudos
Reply