eTSEC1 reset configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eTSEC1 reset configuration

1,588 Views
dank4
Contributor II

i want to set the eTSEC1 at POR to act at MII mode , 

according to Table 3-2 at the P2020RM the cfg_tsec1_prtcl[0,1] are TSEC1_TXD[0,7] signals respectively.

according to Table 4-19 in order to work as MII the POR values should be :

cfg_tsec_reduce = 1 , and cfg_tsec1_prtcl = 01.

it is not clear to me

does that mean cfg_tsec1_prtcl = TSEC1_TXD[0,7] = 01 ?

i would expect the notion to be cfg_tsec1_prtcl[0:1] = 01 

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,541 Views
ufedor
NXP Employee
NXP Employee

prtcl.jpg

1,542 Views
dank4
Contributor II

thank you

0 Kudos
Reply