[e500v2 / e500mc] R^X memory pages support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[e500v2 / e500mc] R^X memory pages support?

2,049件の閲覧回数
davychoplin
Contributor I

Hello,

R^X memory pages support is not common on ARM and x86 architectures, I am wondering if it is the same for QorIQ processors.

When reading the e500v2 and e500mc reference manuals, I have the feeling that it is possible to add TLB with execute only rights (without read / write rights).

Is my understanding correct?

Best regards,

Davy C.

0 件の賞賛
返信
2 返答(返信)

1,857件の閲覧回数
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

For more details please refer to the EREF: A Programmer’s Reference Manual for Freescale Power Architecture Processors, 7.5.8 Permission Attributes.

1,857件の閲覧回数
davychoplin
Contributor I

Thank you for your answer

0 件の賞賛
返信