ddr3 bring up and initialization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ddr3 bring up and initialization

1,836件の閲覧回数
jagxin
Contributor III

DDR_DDR_SDRAM_MODE -how to find this value  to be entered to the register base on dram chip 

1.ESDMODE

2.SDMODE

how qcvs is generating this values ?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,627件の閲覧回数
jagxin
Contributor III

dear sir thanks for your reply

i have created an rcw file for 400mhz ddr3 with p2041 i have created a tcl file with qcvs for the 667 mhz ddr3 controller it is reading and writing fine

if i need to decrease  the the timing to 667 mhz ddr3 by changing the code word and after flashing into the flash i am facing the error of protocol plugin error ,how to fix this ?

0 件の賞賛
返信

1,627件の閲覧回数
Bulat
NXP Employee
NXP Employee

These values are really based on the SDRAM specification, you need to check the datasheet of the SDRAM you are using. For DDR3 memory SDMODE corresponds to Mode Register 0 (MR0) of the SDRAM, ESDMODE - to Mode Register 1 (MR1).

Regards,

Bulat