ddr3 bring up and initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ddr3 bring up and initialization

1,835 Views
jagxin
Contributor III

DDR_DDR_SDRAM_MODE -how to find this value  to be entered to the register base on dram chip 

1.ESDMODE

2.SDMODE

how qcvs is generating this values ?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,626 Views
jagxin
Contributor III

dear sir thanks for your reply

i have created an rcw file for 400mhz ddr3 with p2041 i have created a tcl file with qcvs for the 667 mhz ddr3 controller it is reading and writing fine

if i need to decrease  the the timing to 667 mhz ddr3 by changing the code word and after flashing into the flash i am facing the error of protocol plugin error ,how to fix this ?

0 Kudos
Reply

1,626 Views
Bulat
NXP Employee
NXP Employee

These values are really based on the SDRAM specification, you need to check the datasheet of the SDRAM you are using. For DDR3 memory SDMODE corresponds to Mode Register 0 (MR0) of the SDRAM, ESDMODE - to Mode Register 1 (MR1).

Regards,

Bulat