ddr clock configuration through synchronous mode from external oscillator not from CPU in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ddr clock configuration through synchronous mode from external oscillator not from CPU in u-boot

1,579 次查看
shubhasingh
Contributor I

Hi,

We are having a P1021 based custom board, in which the clock input to DDR is through ddr synchronous mode from external oscillator not from CPU, i want to support this in U-boot.

I am not getting a clue where to make this change in u-boot so that it supports DDR clocking from external oscillator. Can some body please point me out on this.

Regards,

Shubha

标签 (1)
0 项奖励
回复
2 回复数

1,454 次查看
shubhasingh
Contributor I

Thanks.

0 项奖励
回复

1,454 次查看
Bulat
NXP Employee
NXP Employee

Clocking mode of the DDR is set on the board level, u-boot does not require any special change. Specifically the user should set proper 'cfg_ddr_pll[0:2]' POR configuration field in accordance with the input clock source (frequency), see section 4.5.3.2 of the Ref Manual for details.

Regards,

Bulat

0 项奖励
回复