Hi,
We are having a P1021 based custom board, in which the clock input to DDR is through ddr synchronous mode from external oscillator not from CPU, i want to support this in U-boot.
I am not getting a clue where to make this change in u-boot so that it supports DDR clocking from external oscillator. Can some body please point me out on this.
Regards,
Shubha
Clocking mode of the DDR is set on the board level, u-boot does not require any special change. Specifically the user should set proper 'cfg_ddr_pll[0:2]' POR configuration field in accordance with the input clock source (frequency), see section 4.5.3.2 of the Ref Manual for details.
Regards,
Bulat