boot trace32 script setup law for memory controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

boot trace32 script setup law for memory controller

1,562 次查看
viktorkarlsson
Contributor I

Hi

I use a P1020RDB_PD devkit. For debugging i use Laterbach trace32 probe.

My goal is to boot VxWorks 653 hopefully using U-boot.

 

To make one thing at the time my first goal is setup HW with a probe script.

Secondary load at program to ram and execute it.

 

Here come the first issue.

When I enable the Law for the memory controller I lose communication between the probe and the CPU.

 

The script is attached. I´ve taken most of the values from the U-boot setup.

 

I need a extra pair of eyes for this problem.

/V

Original Attachment has been moved to: bootInitP1020RDB_stripped.cmm.zip

标签 (1)
0 项奖励
回复
1 回复

1,413 次查看
viktorkarlsson
Contributor I

Okey I found a initscript on Lauterbach website. with a few modifications I seems to work.

/V

0 项奖励
回复