about p1023 flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about p1023 flash programming

2,244件の閲覧回数
longqiluo
Contributor II

hello,I have a customized board based on P1023RDB,now I have some trouble about falsh burning ,attached is my trouble description,and some wrong messages output in CW10.5.1, could anyone  help me out ? or just tell me how to configure in CW10.5.1 my flash information :32Mx16x1,DDR3L:64Mx16x2,I am sure the power  supplying is good and the POR configuration is rigth too!

Original Attachment has been moved to: Desktop.rar

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,128件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is highly possible that SDRAM does not operate properly in your case. Try to use RAM initialization script in the "Initialize target script" - see attached.

Also it is needed to uncheck the "CCS executable" checkbox - see attached.

In case of further questions please consider creating a Technical Case:

https://community.freescale.com/thread/381898

0 件の賞賛
返信

2,128件の閲覧回数
longqiluo
Contributor II

hello, should  the RAM initialization script   be modified? because  my DDR3L is not same as script,on other hand, the LAW register and OR0 BR0 ,are not my case

0 件の賞賛
返信

2,128件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please consider creating a Technical Case:

https://community.freescale.com/thread/381898

0 件の賞賛
返信