Why is the NAND flash size in P1022DS_init_sram_flash.tcl file 64K ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is the NAND flash size in P1022DS_init_sram_flash.tcl file 64K ?

Jump to solution
1,296 Views
nishad_kamdar
Contributor IV

I am trying to bring up a custom P1022 board which has a 1GB Nand flash connected to P1022.

I referred to the P1022DS, which also has a 1GB Nand flash.

But when i opened the tcl script, the size of the LAW window for the NAND flash is configured to only 64K.

Why is that???

Thanks for your time and support.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,120 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

The NAND flashes aren't memory mapped (as NOR flashes) - for that reason in the intialization (TLB/MMU, LAW, eLBC CS) we're mapping only a small section SRAM eLBC controller used for programming the NAND flash (you can take a look into the processor reference manual for full details).

Regards,

Marius

View solution in original post

0 Kudos
Reply
2 Replies
1,121 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

The NAND flashes aren't memory mapped (as NOR flashes) - for that reason in the intialization (TLB/MMU, LAW, eLBC CS) we're mapping only a small section SRAM eLBC controller used for programming the NAND flash (you can take a look into the processor reference manual for full details).

Regards,

Marius

0 Kudos
Reply
1,120 Views
nishad_kamdar
Contributor IV

Ok, i got it.

Thanks.

0 Kudos
Reply