Using eTSEC2 on a P1010RDB with VxWorks 6.8?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using eTSEC2 on a P1010RDB with VxWorks 6.8?

1,495 次查看
sopgenorth
Contributor II

Hello,

I'm attempting to configure eTSEC2 on the P1010RDB for use in my application. Currently I have all three of the eTSEC ports configured in my kernel configuration (for VxWorks 6.8), and seen ARP requests get sent from eTSEC2 when trying to boot from that port. When this is happening I will even see a proper ARP response from the host/FTP server (with the vxworks image), but the P1010RDB appears to be blind to it. Switching over to using eTSEC1 works without an issue. Does anyone have any suggestions as to why it appears my P1010RDB can send data, but not receive data?

标签 (1)
0 项奖励
回复
1 回复

1,306 次查看
sopgenorth
Contributor II

This was an issue with my VxWorks 6.8 BSP. This issue is resolved by using the latest build of VxWorks 6.9.4.4

0 项奖励
回复