UCC UART Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UCC UART Speed

2,830 Views
naveennaga
Contributor I

Hi All,

We are using p1021 processor in our project. Quick engine UCC will be used as UART in synchronous mode. We want to achieve 2 Mbps  with UCC configured in slow protocol and UART in NSMI mode.

Can we achieve with slow protocol UCC UART? If so can you guide to the register configuration for clock setting and other.

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

2,622 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 17.1, 17.1.3.2 and Table 17-6 of the QUICC Engine Block Reference Manual (https://www.freescale.com/webapp/Download?colCode=QEIWRM&location=null&fpsp=1&WT_TYPE=Reference%20Ma...).

The P1021 UCC UART supports 2 Mbps with UCC configured in slow protocol and UART in NSMI mode.

Freescale offers CPM performance calculator for the MPC82xx (http://www.freescale.com/webapp/sps/download/license.jsp?colCode=MPC8260CALC2&location=null&Parent_n...).

This calculator can be used as lower estimation UCC UART.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,622 Views
naveennaga
Contributor I

Thank You Pavel.

I'm referring the ucc_uart.c low driver code from QorIQ 1.7 SDK to

implement the synchronous UART with enabling RTS,CTS,CD and DTR , DSR ,RI

as gpios .

Is there any sample device tree for enabling these control signals and code

for control of this signals during Tx and Rx.

0 Kudos
Reply

2,622 Views
Pavel
NXP Employee
NXP Employee

Look at the following page:

http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F2151457.html

This driver can be used as example using additional signals of the RS-232.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply