UART P2020-RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART P2020-RDB

1,408件の閲覧回数
hammadnayeem
Contributor II

Pls tell how to write a UART Code using relevant APIs and cross compile it to P2020-RDB using SDK v1.7.

ラベル(1)
0 件の賞賛
返信
1 返信

1,209件の閲覧回数
Pavel
NXP Employee
NXP Employee
Look at the following page for SDK toolchain installing:
http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F3069706.html
 
Use the following command for test.c compiling:
$CC test.c --sysroot=/opt/fsl-networking/QorIQ-SDK-V1.7/sysroots/ppce500v2-fsl-linux-gnuspe/ -o test

There are lot examples in internet for UART using under Linux. For example, see the following page:

http://www.tldp.org/HOWTO/Text-Terminal-HOWTO.html


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信