Setting the External Debug Control Register EDBCR0 (P4080)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting the External Debug Control Register EDBCR0 (P4080)

ソリューションへジャンプ
1,691件の閲覧回数
clemensreibetan
Contributor I

Hi,

I want to set the EDBCR0[EDM] to 0.

How can I do this?

The manual says (E500MCRM, p.329):

Addressing the debug/expert resources through the memory mapped interface entails driving a base

address for the e500mc core (BASE), a functional group select (GID) and register index for a specific

register. The functional group select determines what class of resource is to be accessed, while the register

index determines which resource within the group to access.

Refer to the SoC reference manual for specifics on accessing the internal memory mapped resources via

the external JTAG interface as well as the Aurora high speed serial interface.

What does this mean? (I am using the code warrior tap if this is important)

I hope you can help me.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,532件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

We have colleague provide a way for previous customer asking about this, to control the EDM/IDM mode, while under debugger control. Please check below:


Enter the following command in the Debugger Shell view, while in a debug session:
    protocol ccs::config_template <core_chain_pos> 0 <value>
where
<core_chain_pos> is the chain position of the core for which you need to alter the EDM mode, eg 1 for core#0, 2 for core#1 etc
<value> is according to the following table:
  /* EDM: External Debug Mode.  Default value is 1. Values mean:
    * 0: EDM off when running, off when stepping
    * 1: EDM on when running, on when stepping
    * 2: EDM on when running, off when stepping
    * 3: EDM off when running, on when stepping


Please note changing this mode can break CW debugger's functionality.



Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,533件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

We have colleague provide a way for previous customer asking about this, to control the EDM/IDM mode, while under debugger control. Please check below:


Enter the following command in the Debugger Shell view, while in a debug session:
    protocol ccs::config_template <core_chain_pos> 0 <value>
where
<core_chain_pos> is the chain position of the core for which you need to alter the EDM mode, eg 1 for core#0, 2 for core#1 etc
<value> is according to the following table:
  /* EDM: External Debug Mode.  Default value is 1. Values mean:
    * 0: EDM off when running, off when stepping
    * 1: EDM on when running, on when stepping
    * 2: EDM on when running, off when stepping
    * 3: EDM off when running, on when stepping


Please note changing this mode can break CW debugger's functionality.



Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信