Sector Protection Error when program flash on t4240qds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sector Protection Error when program flash on t4240qds

9,069件の閲覧回数
p4080ds
Contributor I

Hi,

   I tried to program nor flash on a t4240qds bareboard via CodeWarrior TAP, but got following error.

   I added an unprotect , an erase  and a program action. I'm sure the qds board is good.

fl::target -lc "test_RAM_T4240_Download"

fl::target -b 0x0 0x180000

fl::target -v off -l off

cmdwin::fl::device -d "S29GL01GP" -o "64Mx16x1" -a 0xe8000000 0xefffffff

cmdwin::fl::protect all off

Beginning Operation ...   

-------------------------

Performing target initialization ...   

Downloading Flash Diagnostics Driver ...  

Reading flash ID ...

Unprotecting all sectors...  

Unprotecting ...  

Unprotecting ....  

Unprotecting .....  

Unprotecting ......  

Unprotect Command Succeeded   

cmdwin::fl::device -d "S29GL01GP" -o "64Mx16x1" -a 0xe8000000 0xefffffff

cmdwin::fl::device -sd all

cmdwin::fl::device -se 0

cmdwin::fl::erase list

-------------------------

Downloading Flash Device Driver ...  

Reading flash ID ...

Erasing Sector 0xE8000000 to 0xE801FFFF  

Erasing ...

Error:  Erase failed.   Flash driver reports the following error(s):  Sector Protection Error

Error: Erase failed. Flash driver reports the following error(s):  Sector Protection Error

Any help will be appreciated.

   Regards,

     weiqiang

0 件の賞賛
返信
7 返答(返信)

7,361件の閲覧回数
uvmbox
Contributor III

I have the same problem. How can i solve it? I can erase flash, but i cant write data.

pastedImage_2.png

0 件の賞賛
返信

7,361件の閲覧回数
longqiluo
Contributor II

hello, do you solved this problem?  what reason causes this error?

0 件の賞賛
返信

7,361件の閲覧回数
addiyi
NXP Employee
NXP Employee

Instead of adding Erase action for sector, you must use Program Action with Erase sectors before program.

Adrian

0 件の賞賛
返信

7,359件の閲覧回数
p4080ds
Contributor I

Hi Adrian,

  Thank you for your patience to answer.

   I also tried the way which you metioned above, but still show me Sector Protection Error.This is very confusing. Is there any other helpful tips I missed?

sectorerror.png

        Thanks,

    Weiqiang

0 件の賞賛
返信

7,359件の閲覧回数
addiyi
NXP Employee
NXP Employee

Did you check 'Restricted Addresses in this Range' option? Also, make sure you use the init when connecting to board.

Adrian

0 件の賞賛
返信

7,359件の閲覧回数
p4080ds
Contributor I

Yes, I checked this option.

range.png

0 件の賞賛
返信

7,359件の閲覧回数
addiyi
NXP Employee
NXP Employee

This option will restrict actions on that memory zone. You don't have to use this option, just use Erase before programming and eventually the Address Offset.

Adrian

0 件の賞賛
返信