The changes are relative to the 3.8.13-rt9 kernel based on the SDK1.5 that the board manufacturer provided us with. This kernel works mostly fine, in fact I am using Iceweasel on the board to post this.
I have pasted my dmesg here:
http://pastebin.com/wWVbGU3W
You can see the Radeon DRM driver is failing on a ring test, this happens with >3.5M ram enabled, one of the reason I want to move on to a newer kernel.
And here is the output from a default SDK1.7 kernel:
http://pastebin.com/aqzHmcPA
The supplied source does have an additional file to provide board initialisation, it's beginning to sound like more was patched than I thought.
FYI, this is the same board AlexPerez has been having trouble with.
Hope this makes things clearer.
Thanks
Darren