Reference Schematics/Design files for P1015/P1024 development board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reference Schematics/Design files for P1015/P1024 development board?

ソリューションへジャンプ
1,476件の閲覧回数
fibu
Contributor I

We are going to use NXP P1015 processor in our design. We are also planning to buy its development board:

QorIQ P1024/P1015 Reference Design|NXP 

But I could not find any design resources for this. Usually NXP provides design files for their development boards (For example iMX6). So where could I find these design files?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,279件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The nxp website contains documentation including the P1025RDB specifications document

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...

The board is supplied with a DVD disk or memory stick which contains schematic and software. In any case, you can send request for the design material to the tech. support. See How I could create a Service Request?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,280件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The nxp website contains documentation including the P1025RDB specifications document

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...

The board is supplied with a DVD disk or memory stick which contains schematic and software. In any case, you can send request for the design material to the tech. support. See How I could create a Service Request?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------