Received Packets Not Transferred from FMan Memory to DDR RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Received Packets Not Transferred from FMan Memory to DDR RAM

1,895件の閲覧回数
daniel_will
Contributor I

Hello All,

I am developing bare-metal Ethernet driver software on an XPedite5470 board with the P5020 processor.  In this software, I am configuring dTSEC5 for Ethernet Independent mode receive and transmit processing.  After dTSEC5, FMan, and the PHY device are initialized, auto-negotiation successfully completes and a link is present as reported by the PHY device.  At this point, it appears that the MAC is receiving packets because I see the packets’ data stored in the FMan buffer pool memory, but the data is not transferred to DDR RAM, the Offset In field in the RxQD is not advanced to the next RX buffer descriptor, and the Empty bit is not cleared in the current RX buffer descriptor.

When compared to the dTSEC5/FMan configuration performed by UBoot, where proper dTSEC5 RX port operation was observed (packet data was transferred to DDR RAM with the RxQD and RX BD fields updated correctly), I believe my driver software is correct; however, I have to be missing something.  Any help on this matter would be appreciated.

Here are the parameters of my dTSEC5/FMan configuration:

dTSEC5 Registers:

- ECNTRL = 0x00001050

- MACCFG1 = 0x0000000F

- MACCFG2 = 0x00007215

- RCTRL = 0x00000001

- MAXFRM = 0x00000800

 

BMI Common Registers:

- FMBM_CFG1 = 0x01FF0010

- FMBM_CFG2 = 0x00600018 (reset value)

- FMBM_PP_12 (port parameters for dTSEC5 RX) = 0x03000000

- FMBM_PFS_12 (FIFO parameters for dTSEC5 RX) = 0x0000000F

 

BMI dTSEC5 RX Registers:

- FMBM_RCFG = 0x81000000

- FMBM_RDA = 0 (reset value)

- FMBM_RFP = 0x03FF03FF (reset value)

- FMBM_RICP = 0x00000002 (reset value)

- FMBM_RIM = 0 (reset value)

- FMBM_REBM = 0x00020000 (reset value)

- FMBM_RFNE = 0x0000000A

- FMBM_RFCA = 0x003C0000

- FMBM_RFPNE = 0x00480000

- FMBM_RFQID = 0x00021200

- FMBM_SPLIODN = 0x0000000E

 

FMan DMA registers:

- FMDM_MR = 0x10006800

- FMDM_TR = 0x18600060 (reset value)

- FMDM_HY = 0x10400040 (reset value)

- FMDM_PLR6 (for dTSEC5 RX port) = 0x00200020

 

The following information represents dTSEC5 and FMan status after the reception of several packets.

Parameter RAM dump for the dTSEC5 RX port (note that the CCSR address is 0x0_8000_0000):

0080421200  20000000  00021220  00000000  000B0000         

0080421210  00000000  00000000  00000000  00000000         

0080421220  00000000  70000100  00800000  00000000          <-- Offset In field not advanced

0080421230  00000000  00000000  00000000  00000000         

0080421240  00000000  00000000  00000000  00000000         

0080421250  00000000  00000000  00000000  00000000         

0080421260  00000000  00000000  00000000  00000000         

 

RX Buffer Descriptor Ring dump for the dTSEC5 RX port:

0070000100  80000000  00000000  00000000  70010200          <-- Empty bit not cleared

0070000110  80000000  00000000  00000000  70010A00         

0070000120  80000000  00000000  00000000  70011200         

0070000130  80000000  00000000  00000000  70011A00         

0070000140  80000000  00000000  00000000  70012200         

0070000150  80000000  00000000  00000000  70012A00         

0070000160  80000000  00000000  00000000  70013200         

0070000170  80000000  00000000  00000000  70013A00         

0070000180  08000000  00000000  00000000  00000000         

0070000190  00000000  00000000  00000000  00000000         

 

First receive buffer (referenced by first RX BD):

0070010200  00000000  00000000  00000000  00000000         <-- Packet data not transferred from FMan memory

0070010210  00000000  00000000  00000000  00000000         

0070010220  00000000  00000000  00000000  00000000         

0070010230  00000000  00000000  00000000  00000000         

0070010240  00000000  00000000  00000000  00000000         

0070010250  00000000  00000000  00000000  00000000         

0070010260  00000000  00000000  00000000  00000000          

0070010270  00000000  00000000  00000000  00000000         

0070010280  00000000  00000000  00000000  00000000         

 

BMI RX registers:

- FMBM_RFRC = 0x00000004 (increments by one after each received packet until the value shown is reached, regardless of the number of received packets)

- FMBM_RBFC = FMBM_RLFC = FMBM_RFFC = FMBM_RFDC = FMBM_RFLDEC = FMBM_RODC = FMBM_RBDC = 0

 

FMan DMA registers:

- FMDM_SR = 0

- FMDM_TCID = 0

 

dTSEC5 MIB Counter registers:

- RBYT = 0x00000588

- RPKT = 21

- RCFS = 0

- RMCA = 1

- RBCA = 20

- RXCF = RXPF = RXUO = RALN = RFLR = RCDE = RCSE = RUND = ROVR =RFRG = RJBR = 0

- RDRP = 4

 

Please let me know if I’ve omitted anything.

Thanks in advance,

Daniel

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,644件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Daniel Will,

Please refer to the attached FMAN driver which I got from NetComm 4.7.

Please refer to ./FM/MAC/dtsec.h and ./FM/Port/fm_port.h.

NetComm is a bare board project driver package, it can be downloaded from from NetComm Software Resources|NXP .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信