Query regarding P1022 TSEC GTX clock pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query regarding P1022 TSEC GTX clock pin

ソリューションへジャンプ
1,685件の閲覧回数
prasantahalder
Contributor II

I have two question during design with P1022-

1. We are using One TSEC of P1022 in RGMII mode. Should we provide 125MHz clock in TSEC1_GTX_CLK125 pin? What should be it's source - Oscillator or external @PHY recovered clock?

2. We are using serdes1 for on 2xPCIe and one SGMII and serdes2 disabled. We provided 100MHz in SD1_REF_CLK pin and SD2_REF_CLK is grounded. Is the scheme correct or do we need to provide clock in SD2_REF_CLK pins as well?

ラベル(1)
タグ(2)
1 解決策
1,506件の閲覧回数
bpe
NXP Employee
NXP Employee

TSECn_GTX_CLK125 is the reference clock in RGMII mode. You must provide

this clock to the TSEC that is in RGMII mode. It can be taken from any source

that satisfies the requirements of the chip Hardware Specification.

As of the reference clock to the unused SerDes bank, yes, ground the

inputs.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,507件の閲覧回数
bpe
NXP Employee
NXP Employee

TSECn_GTX_CLK125 is the reference clock in RGMII mode. You must provide

this clock to the TSEC that is in RGMII mode. It can be taken from any source

that satisfies the requirements of the chip Hardware Specification.

As of the reference clock to the unused SerDes bank, yes, ground the

inputs.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------