Queries regarding P1013 Microprocessor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Queries regarding P1013 Microprocessor

1,964件の閲覧回数
lokeshe
Contributor I

Hi,

In one of our project we are using P1013 Microprocessor for Ethernet Module. My question is:-

if I connect 8 port switch IC#1 on RGMII#1 and 8 port Switch IC#2 on RGMII#2/PCIe then all 16 ports are able to exchange data?.

Please find the attached block diagram for easier understanding.

Please revert back asap.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,839件の閲覧回数
LPP
NXP Employee
NXP Employee

P1013 doesn't provide hardware support for automatic mapping of Ethernet packets between RGMII ports or Ethernet modules on PCIe. This mapping can be implemented by means of software.

Linux SDK provides reproducibility guides how to perform benchmarking of IPv4 forward, IPSec forward, NAT and Firewall (eTSEC version). These tests applicable to P1022/P1013.

http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F5074421.html


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,839件の閲覧回数
lokeshe
Contributor I

Thanks for the information. Can you please confirm whether Mapping can be done between 1 RGMII port and PCIe.

0 件の賞賛
返信