QoriQ DDR controller input AC timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QoriQ DDR controller input AC timing

2,470 Views
fjullien
Contributor II

Hi,

In the P1020 datasheets, the only AC parameter regarding the input timings is tDISKEW (and tCISKEW which is almost the same).

This parameter gives the amount of skew consumed by the controller between MDQS and MDQ/MECC.

It says this value should be substracted from the total timing budget. However, don't we need the input setup and hold time to

determine the timing budget at the controller input ?

I can't find any information about the timing relationship between MCK and DQS (like tDQSS and tDQSCK on the memory side).

Is this something we don't need to know ? Am I missing something ?

Thanks in advance for your help.

Franck.

Labels (1)
Tags (4)
0 Kudos
Reply
2 Replies

2,254 Views
lunminliang
NXP Employee
NXP Employee

I am afraid tCISKEW is the only requirement for DQ/DQS input, setup and hold time are due to DQS to DQ skew.

CPO auto-calibration adjusts the time when the the DDR controller expects DQS preamble from the SDRAM. MCK does not matter.

2,254 Views
fjullien
Contributor II

Thank you for those informations.

Franck.

0 Kudos
Reply