QoriQ DDR controller input AC timing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QoriQ DDR controller input AC timing

1,653 次查看
fjullien
Contributor II

Hi,

In the P1020 datasheets, the only AC parameter regarding the input timings is tDISKEW (and tCISKEW which is almost the same).

This parameter gives the amount of skew consumed by the controller between MDQS and MDQ/MECC.

It says this value should be substracted from the total timing budget. However, don't we need the input setup and hold time to

determine the timing budget at the controller input ?

I can't find any information about the timing relationship between MCK and DQS (like tDQSS and tDQSCK on the memory side).

Is this something we don't need to know ? Am I missing something ?

Thanks in advance for your help.

Franck.

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

1,437 次查看
lunminliang
NXP Employee
NXP Employee

I am afraid tCISKEW is the only requirement for DQ/DQS input, setup and hold time are due to DQS to DQ skew.

CPO auto-calibration adjusts the time when the the DDR controller expects DQS preamble from the SDRAM. MCK does not matter.

1,437 次查看
fjullien
Contributor II

Thank you for those informations.

Franck.

0 项奖励
回复