QorIQ Linux SDK v2.0 supported P1020 ??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ Linux SDK v2.0 supported P1020 ??

Jump to solution
1,270 Views
alvinhsu
Contributor II

QorIQ SDK v2.0 - Release Notes says that P1010, P1021/2/3/4/5, P2020/10, and BSC9131/2 no longer supported. Please see prior SDK releases and support in upstream repositories. Does it mean P1020 also no supported ?? (P1010 and P1020 is in the same family series)

Labels (1)
1 Solution
1,017 Views
alvinhsu
Contributor II

I have found that somebody has the same question.

https://community.nxp.com/thread/399212#comments

View solution in original post

0 Kudos
Reply
2 Replies
1,017 Views
Pavel
NXP Employee
NXP Employee

There is the following list in SDK 2.0.

    Supported machines:

    b4420qds-64b b4420qds b4860qds-64b b4860qds c293pcie

                ls1021atwr ls1043aqds ls1043ardb ls2080ardb

                p2041rdb p3041ds p4080ds p5020ds-64b p5020ds p5040ds-64b p5040ds

                t1023rdb-64b t1023rdb t1024rdb-64b t1024rdb t1040d4rdb-64b t1040d4rdb t1042d4rdb-64b

                t1042d4rdb t2080qds-64b t2080qds t2080rdb-64b t2080rdb t4160qds-64b t4160qds

                t4240qds-64b t4240qds t4240rdb-64b t4240rdb

Use SDK 1.9 for the P1010.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,018 Views
alvinhsu
Contributor II

I have found that somebody has the same question.

https://community.nxp.com/thread/399212#comments

0 Kudos
Reply