QCVS TOOL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS TOOL

1,834件の閲覧回数
yansongzhu
Contributor III

When I use the QCVS Tool to configure DDR2 which on the P2020 board, the default configuration of DQS# is disabled. I must enable it by myself. I want to know that if I set bit10 of EMR1 register to 0, has the DQS# signal been enabled ? 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,640件の閲覧回数
ufedor
NXP Employee
NXP Employee

P2020 supports only differential DQS - refer to the P2020 RM, 8.4.9 DDR SDRAM control configuration 2 (DDR_DDR_SDRAM_CFG_2), 4–5 DQS_CFG.

> if I set bit10 of EMR1 register to 0, has the DQS# signal been enabled ?

The DQS# will be enbled for the DDR2 SDRAM chips.

0 件の賞賛
返信