Problem in configurating eTSEC2 to RGMII mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem in configurating eTSEC2 to RGMII mode

跳至解决方案
6,202 次查看
prasantahalder
Contributor II

Hi,

We are using both eTSECs of P1022 in RGMII mode in our custom board. The problem we are facing is with eTSEC2 which is connected to Marvell's RGMII to Copper PHY(88E1510). From PHY LEDs and MII registers, we have found the link is up and autonegotiation complete. But when we are trying to ping from U-BOOT, we are getting "eTSEC2 : tsec: tx error" and then "eTSEC2 : tsec: tx buffers full".

We have checked the POR value of cfg_tsec1_prtc, cfg_tsec2_prtc and cfg_serdes_ports are 1, 1 and "11111" respectively. We have the following questions on this -

1. What could be the possible reason for this ping failure?

2. We have only fed 125MHz clock from a oscillator in TSEC1_GTX_CLK125. Whereas TSEC2_GTX_CLK125 is kept floating. In GUTs_PMUXCR[1588_USB_PWRFIT] is set to GPIO_1 (i.e. 11). Do we need any other registers to be set  for TSEC1_GTX_CLK125 to feed both eTSEC1 and eTSEC2?

3. Another doubt is the autonegotiation result is 100BaseT FDX, whereas it should be 1000BaseT as the link partner is advertising all 10/100/1000BaseT.

Regards,

Prasanta

标签 (1)
0 项奖励
回复
1 解答
5,627 次查看
prasantahalder
Contributor II

Thanks for your help. During debugging, we found that some of the "Misc Debug and Test Interface Pin" were set to low during reset in our board. After correcting this the eTSEC problem disappeared.

在原帖中查看解决方案

0 项奖励
回复
10 回复数
5,627 次查看
shaileshpanchal
Contributor I

Hi , We are using eTSEC1 and eTSEC3 of P1020 in RGMII mode in custom board. We are facing similarly problem "eTSEC1 : tsec: tx error" and then "eTSEC1 : tsec: tx buffers full". 

Please could you shared solution how you over come the above problem. 

0 项奖励
回复
5,627 次查看
prasantahalder
Contributor II

Hi Shailesh,

Check all the POR pins state during out of reset state. In our case, some  "Misc Debug and Test Interface Pin" were set to low during reset in our board. It was causing the problem.

Regards,

Prasanta

0 项奖励
回复
5,627 次查看
prasantahalder
Contributor II

Actually, we have taken the raw dump from uboot prompt after ping failed. During ping the MACCFG1=0x0000_0005 and MACCFG2=0000_7205.

0 项奖励
回复
5,627 次查看
ufedor
NXP Employee
NXP Employee

Absence of Syncd_Rx_EN and Syncd_Tx_EN means that corresponding Ethernet controller does not receive its RX and TX clocks.

What is PORDEVSR value?

0 项奖励
回复
5,628 次查看
prasantahalder
Contributor II

Thanks for your help. During debugging, we found that some of the "Misc Debug and Test Interface Pin" were set to low during reset in our board. After correcting this the eTSEC problem disappeared.

0 项奖励
回复
5,626 次查看
prasantahalder
Contributor II

Hi,

Please find attached the eTSEC1 dump. However we are not currently using eSEC1.

Regards,

Prasanta

0 项奖励
回复
5,626 次查看
ufedor
NXP Employee
NXP Employee

Why Rx_EN and Tx_EN are not set in the MACCFG1?

0 项奖励
回复
5,625 次查看
prasantahalder
Contributor II

Hi,

1. PMUXCR = 0x8000_1000 and PMUXCR2 = 0xFF00_0000

2. File attached

3. SDK version 1.8

4. We are running the ping test in uboot. So, we are currently using any DTS.

Regards,

Prasanta

0 项奖励
回复
5,625 次查看
ufedor
NXP Employee
NXP Employee

Please provide raw memory dump of the initialized eTSEC1 also.

0 项奖励
回复
5,625 次查看
ufedor
NXP Employee
NXP Employee

Please provide additional information:

1) PMUXCR value

2) complete raw memory dump of the initialized eTSEC2

3) which NXP Linux SDK version is used?

4) which DTS is used?

0 项奖励
回复