Parallel NOR flash UBoot settings for P2040 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Parallel NOR flash UBoot settings for P2040 processor

1,606 Views
gouravjain
Contributor IV

Hello All,

Anybody has any lead to how to do settings for Parallel NOR flash UBoot for P2040 processor???? Pls suggest some useful links or pdf

Positive help in tis matter would be highly appreciated..

Rgds,

Gourav

Labels (1)
0 Kudos
Reply
2 Replies

1,391 Views
lunminliang
NXP Employee
NXP Employee

What settings you are asking? Is this on Freescale demo board or customer board?

You could refer to Freescale Technical Information Center for some P2041 hardware and software configuration:

Freescale Technical Information Center

Freescale Technical Information Center

0 Kudos
Reply

1,391 Views
gouravjain
Contributor IV

Hi,

Actually In our card we have P2040 processor and i want to fuse UBoot into that. So I downloaded Uboot and checking files and all. So i got one file inside the configs folder like P2041rdb.h. This files contains all the configuration info. and several macros are also there.

So my first concern is how to understand there macros???

Secondly, we are trying to boot processor from NOR flash so is there any application not or relevant docs which can give NOR sequencing steps and which essential files are required like AN3201 is available for NAND flash.

thanks in advance :smileyhappy:

rgds,

Gourav jain

0 Kudos
Reply