I am working on the firmware for the P4080DS Expedition. I replaced the u-boot, RCW, and fman-ucode. However now the Ethernet does not work. The entire u boot prompt is attached. I can boot to the Yocto Linux but the Ethernet still does not work.
Warning: SERDES bank 2 expects reference clock 100MHz, but actual is 125MHz
Net: Fman1: Uploading microcode version 106.2.18
Could not get PHY for P4080DS_MDIO3: addr 4
Failed to connect
Fman2: Uploading microcode version 106.2.18
Could not get PHY for P4080DS_MDIO1: addr 0
Failed to connect
FM1@DTSEC2
Error: FM1@DTSEC2 address not set.
, FM1@TGEC1
Error: FM1@TGEC1 address not set.
, FM2@TGEC1
Error: FM2@TGEC1 address not set.
From this prompt I believe the problem is in the fman-ucode. Any help would be appreciated.
Thanks
James
Original Attachment has been moved to: UBoot-Log.zip