P4080 FPU performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080 FPU performance

1,540件の閲覧回数
johnbono
Contributor I

I've been working with a system that uses a P2020. We began with only data collection but then added embedded processing, requiring double-precision floating-point calculations. Things are working but it's slow, and we would like to upgrade the system. The company that builds the system has suggested switching to a board that uses the P4080.

I've seen the FPU on the P4080 described as "classic," whatever that means. Can anyone give me a rough idea of what kind of performance difference I would see on the DP FP calculations? We're running LInux with RT patches. The main program is multi-threaded. Most of the FP work is done in a series of separate (single-threaded) OS processes.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,297件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following page about e500v2 (P2020) and e500mc (P4080) comparison:

https://en.wikipedia.org/wiki/PowerPC_e500

 

Perhaps e5500 core is better for your task:

http://www.freescale.com.cn/cstory/ftf/2010/pdf/0425.pdf

 

and

 

https://en.wikipedia.org/wiki/PowerPC_e5500

 

See also the following:

http://caxapa.ru/thumbs/651650/WBNR_FTF2014_NET_F0143.pdf

and

http://www.eetimes.com/document.asp?doc_id=1256711


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信