P3041 debug spread spectrum

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3041 debug spread spectrum

1,414 Views
victorjardim
Contributor I

Hello,

In the P3041 Reference Manual, its mentioned that spread spectrum clocking is not supported when using the Debug function in the same SerDes bank. If I feed with spread spectrum clock the SD_REF_CLK pins of a bank which is configured to, among other functions, as Debug, will those other functions stop to work correctly? Or will only the Debug function stop to work correctly? I'm assuming that I'll not use the debug function when the device is in its normal use, so in this situation I might use a spread spectrum clock source.

Thanks

Victor

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
r8070z
NXP Employee
NXP Employee

You should not use a spread spectrum clock source only if you actually use debug function. While you do not use the debug function you can use a spread spectrum clock source even if the bank configuration includes debug.

0 Kudos
Reply