P3041 PCIExpress read/write problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3041 PCIExpress read/write problem.

1,503 Views
dshard
Contributor I

Hello.

I  have problem with read/write memory of device wich is on PCIE bus. I have bases addresses BAR0 = 0xFFC00000, BAR2 = 0xE0000000, and  bits settings of register Command/Status (MemorySpaceEnable and I/OSpaceEnable). Inbound window set on CCSR (by default). When reading phys addresses BAR0(0xFFC00000) garbage returns. When reading write data overrides read only registers. How i can config PCIE Bus correclty?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,271 Views
ufedor
NXP Employee
NXP Employee

> I  have problem with read/write memory of device wich is on PCIE bus.

Is this device P3041?

If "yes" please provide:

1) complete PCI configuration header of the device.

2) binary image of the RCW being used

0 Kudos
Reply