P3041 PCIExpress read/write problem.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3041 PCIExpress read/write problem.

1,463件の閲覧回数
dshard
Contributor I

Hello.

I  have problem with read/write memory of device wich is on PCIE bus. I have bases addresses BAR0 = 0xFFC00000, BAR2 = 0xE0000000, and  bits settings of register Command/Status (MemorySpaceEnable and I/OSpaceEnable). Inbound window set on CCSR (by default). When reading phys addresses BAR0(0xFFC00000) garbage returns. When reading write data overrides read only registers. How i can config PCIE Bus correclty?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,231件の閲覧回数
ufedor
NXP Employee
NXP Employee

> I  have problem with read/write memory of device wich is on PCIE bus.

Is this device P3041?

If "yes" please provide:

1) complete PCI configuration header of the device.

2) binary image of the RCW being used

0 件の賞賛
返信