P2041rdb bare minimum dTSEC ethernet driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2041rdb bare minimum dTSEC ethernet driver

2,448 Views
haider
Contributor II

Hi,

I am trying to write a bare minimum Ethernet driver for the p2041rdb platform.

If anybody can guide to what reference code or documentation should I refer to do this.

I do have the linux SDK and also NetComm source.

I am not sure what will be the best option to move forward as the documentation is really involved. And the above references covers the feature which I don't want in my case.

Thanks,

Haider

Labels (1)
3 Replies

2,121 Views
scottwood
NXP Employee
NXP Employee

U-Boot has an independent mode driver that you may find helpful.

2,121 Views
haider
Contributor II

Thanks Scott,

I also followed the series at [Which talks about the Setting Up Basic Network Drivers using DPAA]

Multicore Expert Series: Programming Data Pat|Freescale

But when I tried to access the DINK32 reference used by this series. I came across disclaimer that DINK32 no longer contain the ethernet driver. Is that right?.

0 Kudos
Reply

2,121 Views
veerendranathj
Contributor III

Hi Haider,

I too have exact requirement ... are you able to implement the DPAA driver for P2041rdb. Please share if you have any reference codes and/or tutorials.

Thanks and Regards,

Veerendranath

0 Kudos
Reply