P2041RDB PCIe Problem . (vxWorks)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2041RDB PCIe Problem . (vxWorks)

2,214 Views
kohyungeun
Contributor I

I have the p2041rdb Borad.

I got the vxWorks BSP from the WindRiber site.

I read a target.ref file. then compiled the bootrom and kernel.

I can the Tffs, SATA, ..

but I can't Pcie.

shell log ->

****************************************************************************************************************************************

>vxBusShow

Registered Bus Types:

  MII_Bus @ 0x002eb1ec

  PCI_Bus @ 0x002eae5c

  PLB_Bus @ 0x002eae78

Registered Device Drivers:

  ppcIntCtlr at 0x002e92c4 on bus PLB_Bus, funcs @ 0x002e92b8

  m85xxTimerDev at 0x002eada8 on bus PLB_Bus, funcs @ 0x002ead8c

  fslSata at 0x002eb2f8 on bus PLB_Bus, funcs @ 0x002eb2e0

  fslDma at 0x002e9f28 on bus PLB_Bus, funcs @ 0x002e9f1c

  epic at 0x002ea0bc on bus PLB_Bus, funcs @ 0x002ea068

  dtsec at 0x002eb0d0 on bus PLB_Bus, funcs @ 0x002eb000

  ns16550 at 0x002ea4a8 on bus PLB_Bus, funcs @ 0x002ea3d8

  ns16550 at 0x002ea460 on bus PCI_Bus, funcs @ 0x002ea3d8

  dtsecMdio at 0x002eb2a0 on bus PLB_Bus, funcs @ 0x002eb274

  genericPhy at 0x002eb234 on bus MII_Bus, funcs @ 0x002eb228

  miiBus at 0x002eb1a4 on bus PCI_Bus, funcs @ 0x002eb148

  miiBus at 0x002eb164 on bus PLB_Bus, funcs @ 0x002eb148

  m85xxPci at 0x002e9e38 on bus PLB_Bus, funcs @ 0x002e9e2c

  m85xxCCSR at 0x002ea134 on bus PLB_Bus, funcs @ 0x002ea128

  QorIQFman at 0x002ea270 on bus PLB_Bus, funcs @ 0x002ea254

  QorIQBman at 0x002ea214 on bus PLB_Bus, funcs @ 0x002ea1f8

  fslGpio at 0x002ea1b8 on bus PLB_Bus, funcs @ 0x002ea19c

  QorIQQman at 0x002ea350 on bus PLB_Bus, funcs @ 0x002ea32c

  QorIQPciEx at 0x002e9edc on bus PLB_Bus, funcs @ 0x002e9e78

  QorIQLaw at 0x002ea2ec on bus PLB_Bus, funcs @ 0x002ea2b0

  plbCtlr at 0x002eaea0 on bus PLB_Bus, funcs @ 0x002eae94

Busses and Devices Present:

  PLB_Bus @ 0x002fe368 with bridge @ 0x002eaee0

    Device Instances:

        ppcIntCtlr unit 0 on PLB_Bus @ 0x002ff328 with busInfo 0x00000000

        epic unit 0 on PLB_Bus @ 0x002ff428 with busInfo 0x00000000

        ns16550 unit 0 on PLB_Bus @ 0x002ff628 with busInfo 0x00000000

        ns16550 unit 1 on PLB_Bus @ 0x002ff828 with busInfo 0x00000000

        ns16550 unit 2 on PLB_Bus @ 0x002ffa28 with busInfo 0x00000000

        ns16550 unit 3 on PLB_Bus @ 0x002ffc28 with busInfo 0x00000000

        fslGpio unit 0 on PLB_Bus @ 0x002ffe28 with busInfo 0x00000000

        QorIQLaw unit 0 on PLB_Bus @ 0x002fff28 with busInfo 0x0

        QorIQBman unit 0 on PLB_Bus @ 0x00300028 with busInfo 0x00000000

        QorIQQman unit 0 on PLB_Bus @ 0x00300128 with busInfo 0x00000000

        QorIQFman unit 0 on PLB_Bus @ 0x00300228 with busInfo 0x00000000

        QorIQPciEx unit 1 on PLB_Bus @ 0x0030d328 with busInfo 0x00000000

        dtsec unit 0 on PLB_Bus @ 0x0030d628 with busInfo 0x0

        dtsec unit 1 on PLB_Bus @ 0x0030d728 with busInfo 0x0

        dtsec unit 2 on PLB_Bus @ 0x0030d828 with busInfo 0x0

        dtsec unit 3 on PLB_Bus @ 0x0030d928 with busInfo 0x0

        dtsec unit 4 on PLB_Bus @ 0x0030da28 with busInfo 0x0

        dtsecMdio unit 0 on PLB_Bus @ 0x0030db28 with busInfo 0x00000000

        m85xxTimerDev unit 0 on PLB_Bus @ 0x0030dc28 with busInfo 0x00000000

        fslSata unit 0 on PLB_Bus @ 0x0030dd28 with busInfo 0x00000000

        fslSata unit 1 on PLB_Bus @ 0x0030de28 with busInfo 0x00000000

        fslDma unit 0 on PLB_Bus @ 0x0030df28 with busInfo 0x00000000

        fslDma unit 1 on PLB_Bus @ 0x0030e028 with busInfo 0x00000000

        miiBus unit 0 on PLB_Bus @ 0x0030e128 with busInfo 0x002fefa8

        miiBus unit 1 on PLB_Bus @ 0x00312328 with busInfo 0x002fef68

        miiBus unit 2 on PLB_Bus @ 0x00312528 with busInfo 0x002fefe8

        miiBus unit 3 on PLB_Bus @ 0x00312728 with busInfo 0x002ff028

        miiBus unit 4 on PLB_Bus @ 0x00312928 with busInfo 0x002ff068

    Orphan Devices:

  MII_Bus @ 0x002fefa8 with bridge @ 0x0030e128

    Device Instances:

        genericPhy unit 0 on MII_Bus @ 0x0030e228 with busInfo 0x00000000

    Orphan Devices:

  MII_Bus @ 0x002fef68 with bridge @ 0x00312328

    Device Instances:

        genericPhy unit 1 on MII_Bus @ 0x00312428 with busInfo 0x00000000

    Orphan Devices:

  MII_Bus @ 0x002fefe8 with bridge @ 0x00312528

    Device Instances:

        genericPhy unit 2 on MII_Bus @ 0x00312628 with busInfo 0x00000000

    Orphan Devices:

  MII_Bus @ 0x002ff028 with bridge @ 0x00312728

    Device Instances:

        genericPhy unit 3 on MII_Bus @ 0x00312828 with busInfo 0x00000000

    Orphan Devices:

  MII_Bus @ 0x002ff068 with bridge @ 0x00312928

    Device Instances:

        genericPhy unit 4 on MII_Bus @ 0x00312a28 with busInfo 0x00000000

    Orphan Devices:

value = 1 = 0x1

-> pciDeviceShow

value = -1 = 0xffffffff

****************************************************************************************************************************************

I used rcw file that rcw_5g_1500mhz.bin (RR_PH_0x19)

Labels (1)
0 Kudos
Reply
1 Reply

1,457 Views
addiyi
NXP Employee
NXP Employee

Hi,

Do you use a custom board? If not, why don't you use SDK 1.4 which is available on freescale.com. Also, you rcw file set PCIe on Slot1 and according with P2041 reference manual, your application should use PCIe2 controller for communication with PCIe device.

SerDes 0x19 -> Bank 1 C: SGMII1, D: SGMII2, E,F: PCIe2, G: SGMII3, H: SGMII4

Adrian

0 Kudos
Reply