P2041RDB-PC USB Boot Kernel Panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2041RDB-PC USB Boot Kernel Panic

1,741件の閲覧回数
gopikrishnan
Contributor III

I was trying to boot my entire system from USB Flash disk. Installed SDK QorIQ-

SDK-V1.8-20150619-yocto.

 

 

I built image for P2041RDB using

 

 

$ bitbake fsl-image-full

 

 

Under tmp/deploy/images/p2041rdb/

I copied

1) uImage--3.12-r0-p2041rdb-20150623072158.bin -> /flash_disk/uImage.bin

2) uImage--3.12-r0-p2041rdb-20150623072158.dtb -> /flash_disk/uImage.dtb

3) Extracted fsl-image-full-p2041rdb.tar.gz -> /flash_disk/

 

 

On u-boot of P2041RDB-PC board

 

 

=> usb start

=> fatload usb 0:0 $loadaddr img/uImage.bin

=> fatload usb 0:0 $fdtaddr img/uImage.dtb

=> setenv usbboot setenv bootargs root=/dev/sdb rw rootdelay=5

console=$consoledev,$baudrate $othbootargs;bootm $loadaddr - $fdtaddr

=> run usbboot

 

 

But endup with kernel painc error Attachment: "err_in_boot.txt"

 

 

Please note that, I tried both root=/dev/sdb and root=/dev/sdb1. The flash disk is not partitioned. So probably root=/dev/sdb would be correct. and the disk was formatted using vFAT filesystem Please correct If I was wrong.

 

 

Thanks in Advance,

Reg,

Gopi Krishnan S

Original Attachment has been moved to: err_in_boot.txt.zip

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,554件の閲覧回数
gopikrishnan
Contributor III

The small mistake I did, I must have used ext2fs

=> usb start

=> ext2load usb 0:0 $loadaddr img/uImage.bin

=> ext2load usb 0:0 $fdtaddr img/uImage.dtb

=> setenv usbboot "setenv bootargs root=/dev/sdb rw rootdelay=5 console=$consoledev,$baudrate $othbootargs;bootm $loadaddr - $fdtaddr"

=> run usbboot

Remember to format flash disk using mkfs.ext2 /dev/sdb1 before deploying root file system.

Reg,

Gopi Krishnan S

0 件の賞賛
返信